Keysight 89600 VSA .NET API
PrecodingResourceBlockGroup Enumeration
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace : PrecodingResourceBlockGroup Enumeration


Glossary Item Box

Specifies the Precoding Resource Block Group for PDSCH and PUSCH

Syntax

Visual Basic (Declaration) 
Public Enum PrecodingResourceBlockGroup 
   Inherits System.Enum
C# 
public enum PrecodingResourceBlockGroup : System.Enum 
C++/CLI 
public enum class PrecodingResourceBlockGroup : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
FourThe precoding resource block group is 4 consecutive physical resource blocks.—
TwoThe precoding resource block group is 2 consecutive physical resource blocks.—
UserDefinedThe precoding resource block group size is defined by users.25.40
WidebandThe precoding resource block group includes all the allocated physical resource blocks.—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Remarks

When applying MIMO precoding matrix to PDSCH, as the MIMO channel response can be different over different frequency range, accordingly the MIMO precoding matrix can be different over different frequency range. According to 38.214-1 5.1.2.3, there are three kinds of precoding resource block groups when applying precoding matrix. They are 2 PRBs, 4 PRBs and wide band. And UE can assume that the precoding within each precoding resource block group is the same.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 25.20

See Also