Parameters
- item
- Positioning Reference Signal (PRS) to remove from the collection
Return Value
True, if the Positioning Reference Signal (PRS) was removed from the collection.Note the first element in the collection cannot be removed because it is the primary Positioning Reference Signal (PRS).
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA Ver 29.40