Keysight 89600 VSA .NET API
PrsNumberOfSymbols Enumeration
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace : PrsNumberOfSymbols Enumeration


Glossary Item Box

Enum values indicating the number of Positioning Reference Signal (PRS) symbols per Positioning Reference Signal (PRS) Resource within a slot

Syntax

Visual Basic (Declaration) 
Public Enum PrsNumberOfSymbols 
   Inherits System.Enum
C# 
public enum PrsNumberOfSymbols : System.Enum 
C++/CLI 
public enum class PrsNumberOfSymbols : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
N12Specifies Positioning Reference Signal (PRS) symbol number as 12 symbol (N12).29.40
N2Specifies Positioning Reference Signal (PRS) symbol number as 2 symbol (N2).29.40
N4Specifies Positioning Reference Signal (PRS) symbol number as 4 symbol (N4).29.40
N6Specifies Positioning Reference Signal (PRS) symbol number as 6 symbol (N8).29.40
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 29.40

See Also