Keysight 89600 VSA .NET API
Periodicity Property
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace > PrsResourceSet Class : Periodicity Property


Glossary Item Box

Gets or sets a value indicating the Positioning Reference Signal (PRS) periodicity in slots.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property Periodicity As Integer
C# 
public abstract int Periodicity {get; set;}
C++/CLI 
public:
abstract property int Periodicity {
   int get();
   void set (    int value);
}

Property Value

Default value is 10 slots.

Remarks

The unit is in the number of slots.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 29.40

See Also