Keysight 89600 VSA .NET API
SequenceId Property
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace > PrsResource Class : SequenceId Property


Glossary Item Box

Gets or sets a value indicating the Positioning Reference Signal (PRS) resource sequence identity.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property SequenceId As Integer
C# 
public abstract int SequenceId {get; set;}
C++/CLI 
public:
abstract property int SequenceId {
   int get();
   void set (    int value);
}

Property Value

The value range is from 0 to 4095. The default value is 0.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 29.40

See Also