Specifies the offset in slots between repeated instances of a Positioning Reference Signal (PRS) Resource corresponding to the same resource ID within a single instance of Positioning Reference Signal (PRS) Resource Set
Syntax
| Visual Basic (Declaration) | |
|---|
Public Enum PrsTimeGap
Inherits System.Enum |
| C++/CLI | |
|---|
public enum class PrsTimeGap : public System.Enum |
Members
Requirements
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA
Ver 29.40
See Also