Keysight 89600 VSA .NET API
PucchMaxCodeRate Enumeration
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace : PucchMaxCodeRate Enumeration


Glossary Item Box

Enum values for maximum code rate for the PUCCH Physical channel.

Syntax

Visual Basic (Declaration) 
Public Enum PucchMaxCodeRate 
   Inherits System.Enum
C# 
public enum PucchMaxCodeRate : System.Enum 
C++/CLI 
public enum class PucchMaxCodeRate : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
ZeroDot08the maximum code rate is 0.08—
ZeroDot15the maximum code rate is 0.15—
ZeroDot25the maximum code rate is 0.25—
ZeroDot35the maximum code rate is 0.35—
ZeroDot45the maximum code rate is 0.45—
ZeroDot60the maximum code rate is 0.60—
ZeroDot80the maximum code rate is 0.80—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 27.40

See Also