Keysight 89600 VSA .NET API
PucchModulationType Enumeration
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace : PucchModulationType Enumeration


Glossary Item Box

Enum values for PUCCH modulation type

Syntax

Visual Basic (Declaration) 
Public Enum PucchModulationType 
   Inherits System.Enum
C# 
public enum PucchModulationType : System.Enum 
C++/CLI 
public enum class PucchModulationType : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
BpskModulation type is BPSK—
QpskModulation type is QPSK—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 23.20

See Also