Keysight 89600 VSA .NET API
DmrsNidZero Property
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace > Pucch Class : DmrsNidZero Property


Glossary Item Box

Gets or sets a value indicating the ID value used for DMRS data scrambling

Syntax

Visual Basic (Declaration) 
Public Overridable Property DmrsNidZero As Integer
C# 
public virtual int DmrsNidZero {get; set;}
C++/CLI 
public:
virtual property int DmrsNidZero {
   int get();
   void set (    int value);
}

Property Value

Default value is 0.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 23.20

See Also