Keysight 89600 VSA .NET API
InitialCyclicShift Property
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace > Pucch Class : InitialCyclicShift Property


Glossary Item Box

Gets or sets initial cyclic shift

Syntax

Visual Basic (Declaration) 
Public Overridable Property InitialCyclicShift As Integer
C# 
public virtual int InitialCyclicShift {get; set;}
C++/CLI 
public:
virtual property int InitialCyclicShift {
   int get();
   void set (    int value);
}

Property Value

Default value is 0. Range of value is 0 through 11.

Remarks

This property is only applicable for PUCCH Format 0 and 1 configuration

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 23.20

See Also