| Visual Basic (Declaration) | |
|---|---|
Public Overridable Property InterlaceZeroIndex As Integer | |
| C# | |
|---|---|
public virtual int InterlaceZeroIndex {get; set;} | |
Property Value
Default value is 0. For numerology 15kHz, the minimum value is 0, the maximum value is 9. For numerology 30kHz, the minimum value is 0, the maximum value is 4This property corresponds to the higher-layer parameter interlace0 in PUCCH-Resource-r16 information element. Multiple interlaces are defined for numerology 15kHz and 30kHz . For Numerology 15kHz, 10 interlaces are defined. For Numerology 30kHz, 5 interlaces are defined. When InterlacedTransmissionEnabled is true, this value indicates the index of the interlace on which this PUCCH is allocated.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA Ver 25.20