Keysight 89600 VSA .NET API
IsPucchEnabled Property
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace > Pucch Class : IsPucchEnabled Property


Glossary Item Box

Gets or sets a value indicating whether the physical channel is marked as enabled.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property IsPucchEnabled As Boolean
C# 
public abstract bool IsPucchEnabled {get; set;}
C++/CLI 
public:
abstract property bool IsPucchEnabled {
   bool get();
   void set (    bool value);
}

Remarks

The default value for this property depends on the physical channel. implementation within a specific BWP implementation.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also