Keysight 89600 VSA .NET API
OccLength Property
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace > Pucch Class : OccLength Property


Glossary Item Box

Gets or sets the OCC length for PUCCH Format 4 sequence generation

Syntax

Visual Basic (Declaration) 
Public Overridable Property OccLength As Integer
C# 
public virtual int OccLength {get; set;}
C++/CLI 
public:
virtual property int OccLength {
   int get();
   void set (    int value);
}

Property Value

Default value is 2. Valid values are 2, 4.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 24.00

See Also