Gets or sets a value indicating the start index of resource block for second hop of PUCCH in case of frequency hopping. This value is applicable when intra-slot frequency hopping is enabled. This property corresponds to L1 parameter
'PUCCH-2nd-hop-PRB'.
Syntax
| Visual Basic (Declaration) | |
|---|
Public Overridable Property SecondHopRBOffset As Integer |
| C# | |
|---|
public virtual int SecondHopRBOffset {get; set;} |
| C++/CLI | |
|---|
public:
virtual property int SecondHopRBOffset {
int get();
void set ( int value);
} |
Property Value
Default value is 0. Range of value is 0 through (
ULBwp.RBNumber -
RBNumber).
Requirements
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA
Ver 23.20
See Also