Keysight 89600 VSA .NET API
SequenceCyclicShiftAutoDetected Property
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace > Pucch Class : SequenceCyclicShiftAutoDetected Property


Glossary Item Box

Gets or sets a value indicating whether the sequence cyclic shift is auto detected during the measurement.

Syntax

Visual Basic (Declaration) 
Public Overridable Property SequenceCyclicShiftAutoDetected As Boolean
C# 
public virtual bool SequenceCyclicShiftAutoDetected {get; set;}
C++/CLI 
public:
virtual property bool SequenceCyclicShiftAutoDetected {
   bool get();
   void set (    bool value);
}

Property Value

Default value is false.

Remarks

This property is only applicable for PUCCH Format 0 configuration

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 28.00

See Also