Keysight 89600 VSA .NET API
Version Property
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace > Pucch Class : Version Property


Glossary Item Box

Gets or sets the specification interpretation to use for PDSCH.

Syntax

Visual Basic (Declaration) 
Public Overridable Property Version As FiveGVersion
C# 
public virtual FiveGVersion Version {get; set;}
C++/CLI 
public:
virtual property FiveGVersion Version {
   FiveGVersion get();
   void set (    FiveGVersion value);
}

Property Value

Default value is Latest.

Remarks

The 3GPP-NR standard is continually evolving, and this property is provided to allow handling the evolving interpretations of PDSCH.
Enum value Interpretation details
FiveGVersion.Fifteen Interprets PBCH DMRS initialization according to version 15.0.0 of 38.211 (2017-12)
FiveGVersion.FifteenDotOne Interprets PDSCH/PBCH DMRS initialization according to version 15.1.0 of 38.211 (2018-03)
FiveGVersion.FifteenDotTwo Interprets PDSCH/PBCH DMRS initialization according to version 15.2.0 of 38.211 (2018-06)
Latest Interprets PBCH/PDSCH/PUCCH DMRS initialization according to version 15.2.0 of 38.211 (2018-09)
NOTE: Supported interpretations will change with future versions of the software, and will be marked obsolete when no longer beneficial. To ensure the latest interpretation is used in future versions of the software for compiled client automation code, please use the Latest value for this property.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 23.20

See Also