Keysight 89600 VSA .NET API
PuschAntennaPort Enumeration
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace : PuschAntennaPort Enumeration


Glossary Item Box

Enum values indicating antenna port selection for PUSCH physical channels.

Syntax

Visual Basic (Declaration) 
Public Enum PuschAntennaPort 
   Inherits System.Enum
C# 
public enum PuschAntennaPort : System.Enum 
C++/CLI 
public enum class PuschAntennaPort : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
Port0Antenna Port 0—
Port1Antenna Port 1—
Port10Antenna Port 10—
Port11Antenna Port 11—
Port12Antenna Port 1228.60
Port13Antenna Port 1328.60
Port14Antenna Port 1428.60
Port15Antenna Port 1528.60
Port16Antenna Port 1628.60
Port17Antenna Port 1728.60
Port18Antenna Port 1828.60
Port19Antenna Port 1928.60
Port2Antenna Port 2—
Port20Antenna Port 2028.60
Port21Antenna Port 2128.60
Port22Antenna Port 2228.60
Port23Antenna Port 2328.60
Port3Antenna Port 3—
Port4Antenna Port 4—
Port5Antenna Port 5—
Port6Antenna Port 6—
Port7Antenna Port 7—
Port8Antenna Port 8—
Port9Antenna Port 9—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 23.20

See Also