| Visual Basic (Declaration) | |
|---|---|
Public MustOverride Function Remove( _ ByVal item As Pusch _ ) As Boolean | |
Parameters
- item
- PUSCH to remove from the collection
Return Value
True, if the PUSCH was removed from the collection.Note the first element in the collection cannot be removed because it is the primary PUSCH.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)