Keysight 89600 VSA .NET API
RemoveAt Method
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace > PuschRateMatchPatternCollection Class : RemoveAt Method


index
Zero-based index of user to remove from the collection

Glossary Item Box

Removes the PuschRateMatchPattern at the indicated index from the collection.

Syntax

Visual Basic (Declaration) 
Public MustOverride Function RemoveAt( _
   ByVal index As Integer _
) As Boolean
C# 
public abstract bool RemoveAt( 
   int index
)
C++/CLI 
public:
abstract bool RemoveAt( 
   int index
) 

Parameters

index
Zero-based index of user to remove from the collection

Return Value

True, if the PuschRateMatchPattern was removed from the collection.

Remarks

Note the first element in the collection cannot be removed.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also