Gets a value indicating the resource block level bitmap in the frequency domain. The length of the bitmap is 275.
Syntax
| Visual Basic (Declaration) | |
|---|
Public MustOverride Function GetResourceBlockBitmap() As BitArray |
| C# | |
|---|
public abstract BitArray GetResourceBlockBitmap() |
| C++/CLI | |
|---|
public:
abstract BitArray^ GetResourceBlockBitmap(); |
Return Value
The current resource block level bitmap in the frequency domain.
Requirements
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
See Also