Gets or sets a value indicating the payload size(bit number) of the HARQ-ACK transmitted on this PUSCH.
Syntax
| Visual Basic (Declaration) | |
|---|
Public Overridable Property CGUciPayloadSize As Integer |
| C# | |
|---|
public virtual int CGUciPayloadSize {get; set;} |
| C++/CLI | |
|---|
public:
virtual property int CGUciPayloadSize {
int get();
void set ( int value);
} |
Property Value
The unit is bit, default value is 7 bits, range is 7~1706 bits. When both HARQ-ACK and CG-UCI are enabled, the total payload size should be less than 1706 bits
Requirements
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA
Ver 26.00
See Also