Keysight 89600 VSA .NET API
CsiPartOneEnabled Property
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace > Pusch Class : CsiPartOneEnabled Property


Glossary Item Box

Gets or sets a value indicating whether CSI(Channel State Information) Part1 bits are transmitted on this PUSCH.

Syntax

Visual Basic (Declaration) 
Public Overridable Property CsiPartOneEnabled As Boolean
C# 
public virtual bool CsiPartOneEnabled {get; set;}
C++/CLI 
public:
virtual property bool CsiPartOneEnabled {
   bool get();
   void set (    bool value);
}

Property Value

Default value is false.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 26.00

See Also