Gets or sets a value indicating the payload size(bit number) of the CSI Part1 transmitted on this PUSCH.
Syntax
| Visual Basic (Declaration) | |
|---|
Public Overridable Property CsiPartOnePayloadSize As Integer |
| C# | |
|---|
public virtual int CsiPartOnePayloadSize {get; set;} |
| C++/CLI | |
|---|
public:
virtual property int CsiPartOnePayloadSize {
int get();
void set ( int value);
} |
Property Value
The unit is bit, default value is 1 bits, range is 1~1706 bits.
Requirements
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA
Ver 26.00
See Also