Keysight 89600 VSA .NET API
DataScramblingId Property
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace > Pusch Class : DataScramblingId Property


Glossary Item Box

Gets or sets the data scrambling ID configured by higher layer. This property is applicable only when NidSource is NidSource.FromHigherLayer

Syntax

Visual Basic (Declaration) 
Public Overridable Property DataScramblingId As Integer
C# 
public virtual int DataScramblingId {get; set;}
C++/CLI 
public:
virtual property int DataScramblingId {
   int get();
   void set (    int value);
}

Property Value

Default value is 0. Range is from 0 through 65535.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 23.20

See Also