Keysight 89600 VSA .NET API
DmrsMappingTypeAPosition Property
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace > Pusch Class : DmrsMappingTypeAPosition Property


Glossary Item Box

Gets or sets a value indicating the DMRS position when using mapping type A.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property DmrsMappingTypeAPosition As DmrsMappingTypeAPosition
C# 
public abstract DmrsMappingTypeAPosition DmrsMappingTypeAPosition {get; set;}
C++/CLI 
public:
abstract property DmrsMappingTypeAPosition DmrsMappingTypeAPosition {
   DmrsMappingTypeAPosition get();
   void set (    DmrsMappingTypeAPosition value);
}

Property Value

Default value is DmrsMappingTypeAPosition.Pos3.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also