Gets or sets a value indicating the relative power boosting (in dB) of the DMRS associated with this physical channel.
Syntax
| Visual Basic (Declaration) | |
|---|
Public MustOverride Property DmrsPowerBoosting As Double |
| C# | |
|---|
public abstract double DmrsPowerBoosting {get; set;} |
| C++/CLI | |
|---|
public:
abstract property double DmrsPowerBoosting {
double get();
void set ( double value);
} |
Property Value
Default value is 0.0 dB.
Remarks
Requirements
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
See Also