Gets a value indicating the RBG allocation custom bitmap in the frequency domain, which is defined for the case of RBG size = 1RB. The length of the bitmap is
ULBwp.RBNumber RB.
Syntax
| Visual Basic (Declaration) | |
|---|
Public Overridable Function GetRbgAllocationCustomBitmap() As BitArray |
| C# | |
|---|
public virtual BitArray GetRbgAllocationCustomBitmap() |
| C++/CLI | |
|---|
public:
virtual BitArray^ GetRbgAllocationCustomBitmap(); |
Return Value
The user defined RBG allocation custom bitmap
Remarks
Requirements
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA
Ver 28.60
See Also