Gets or sets a value indicating whether the DMRS sequence hopping is On or Off when the PUSCH transform precoding is enabled.
Syntax
| Visual Basic (Declaration) | |
|---|
Public Overridable Property IsDmrsSequenceHoppingEnabled As Boolean |
| C# | |
|---|
public virtual bool IsDmrsSequenceHoppingEnabled {get; set;} |
| C++/CLI | |
|---|
public:
virtual property bool IsDmrsSequenceHoppingEnabled {
bool get();
void set ( bool value);
} |
Property Value
The default value is false.
Requirements
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA
Ver 23.20
See Also