Keysight 89600 VSA .NET API
IsHalfPiBpskSupported Property
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace > Pusch Class : IsHalfPiBpskSupported Property


Glossary Item Box

Gets or sets a value indicating whether the PUSCH support PI/2 BPSK modulation when transform precoding is on.

Syntax

Visual Basic (Declaration) 
Public Overridable Property IsHalfPiBpskSupported As Boolean
C# 
public virtual bool IsHalfPiBpskSupported {get; set;}
C++/CLI 
public:
virtual property bool IsHalfPiBpskSupported {
   bool get();
   void set (    bool value);
}

Property Value

The default value is true.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 23.20

See Also