Gets or sets a value indicating if the PUSCH ID when transform precoding is enabled.
Syntax
| Visual Basic (Declaration) | |
|---|
Public Overridable Property PuschIdentity As Integer |
| C# | |
|---|
public virtual int PuschIdentity {get; set;} |
| C++/CLI | |
|---|
public:
virtual property int PuschIdentity {
int get();
void set ( int value);
} |
Property Value
The default value is false.
Requirements
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA
Ver 23.20
See Also