Gets or sets a value indicating a scaling factor to limit the number of resource elements assigned to UCI(uplink control information) on PUSCH for DCI formats other than DCI format 0_2.
Syntax
Property Value
Default value is 0.5. Value ZeroDotFive corresponds to 0.5, value ZeroDotSixFive corresponds to 0.65, and so on.
Requirements
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA
Ver 26.00
See Also