Keysight 89600 VSA .NET API
XOverhead Property
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace > Pusch Class : XOverhead Property


Glossary Item Box

Gets or sets a value indicating the resource allocation overhead used for CSI-RS and CORESETTransportBlockSize.

Syntax

Visual Basic (Declaration) 
Public Overridable Property XOverhead As XOverhead
C# 
public virtual XOverhead XOverhead {get; set;}
C++/CLI 
public:
virtual property XOverhead XOverhead {
   XOverhead get();
   void set (    XOverhead value);
}

Property Value

Default value is XOverhead.Zero, so no account for CSI-RS and CORESET when calculating the TransportBlockSize .

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 24.20

See Also