Keysight 89600 VSA .NET API
PxschAntennaPort Enumeration
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace : PxschAntennaPort Enumeration


Glossary Item Box

Enum values indicating antenna port selection for the PUSCH or PDSCH physical channel.

Syntax

Visual Basic (Declaration) 
Public Enum PxschAntennaPort 
   Inherits System.Enum
C# 
public enum PxschAntennaPort : System.Enum 
C++/CLI 
public enum class PxschAntennaPort : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
Port1000Antenna Port 1000—
Port1001Antenna Port 1001—
Port1002Antenna Port 1002—
Port1003Antenna Port 1003—
Port1004Antenna Port 1004—
Port1005Antenna Port 1005—
Port1006Antenna Port 1006—
Port1007Antenna Port 1007—
Port1008Antenna Port 1008—
Port1009Antenna Port 1009—
Port1010Antenna Port 1010—
Port1011Antenna Port 1011—
Port1012Antenna Port 101228.60
Port1013Antenna Port 101328.60
Port1014Antenna Port 101428.60
Port1015Antenna Port 101528.60
Port1016Antenna Port 101628.60
Port1017Antenna Port 101728.60
Port1018Antenna Port 101828.60
Port1019Antenna Port 101928.60
Port1020Antenna Port 102028.60
Port1021Antenna Port 102128.60
Port1022Antenna Port 102228.60
Port1023Antenna Port 102328.60
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 23.00

See Also