Keysight 89600 VSA .NET API
RankNumber Enumeration
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace : RankNumber Enumeration


Glossary Item Box

Enum values indicating the rank number of the channel coding of a physical channel.

Syntax

Visual Basic (Declaration) 
Public Enum RankNumber 
   Inherits System.Enum
C# 
public enum RankNumber : System.Enum 
C++/CLI 
public enum class RankNumber : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
EightRank is 8.28.60
FiveRank is 5.28.60
FourRank is 4.—
OneRank is 1.—
SevenRank is 7.28.60
SixRank is 6.28.60
ThreeRank is 3.—
TwoRank is 2.—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 23.00

See Also