Keysight 89600 VSA .NET API
RateMatchPatternLevel Enumeration
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace : RateMatchPatternLevel Enumeration


Glossary Item Box

Enum value indicating the rate match pattern level where a rate match pattern exists.

Syntax

Visual Basic (Declaration) 
Public Enum RateMatchPatternLevel 
   Inherits System.Enum
C# 
public enum RateMatchPatternLevel : System.Enum 
C++/CLI 
public enum class RateMatchPatternLevel : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
BwpLevelThe rate match pattern is defined on the BWP level.—
CellLevelThe rate match pattern is defined on the cell level.—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 26.00

See Also