Keysight 89600 VSA .NET API
RateMatchPatternSubcarrierSpacing Enumeration
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace : RateMatchPatternSubcarrierSpacing Enumeration


Glossary Item Box

Enum value indicating the subcarrier spacing of a rate match pattern.

Syntax

Visual Basic (Declaration) 
Public Enum RateMatchPatternSubcarrierSpacing 
   Inherits System.Enum
C# 
public enum RateMatchPatternSubcarrierSpacing : System.Enum 
C++/CLI 
public enum class RateMatchPatternSubcarrierSpacing : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
Scs120Subcarrier scaling 15kHz corresponds to numerology (µ = 3).—
Scs15Subcarrier scaling 15kHz corresponds to numerology (µ = 0).—
Scs30Subcarrier scaling 15kHz corresponds to numerology (µ = 1).—
Scs480Subcarrier scaling 15kHz corresponds to numerology (µ = 5).27.40
Scs60Subcarrier scaling 15kHz corresponds to numerology (µ = 2).—
Scs960Subcarrier scaling 15kHz corresponds to numerology (¶ = 6).27.40
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 26.00

See Also