| Visual Basic (Declaration) | |
|---|---|
Public Overloads MustOverride Function Remove() As Boolean | |
| C# | |
|---|---|
public abstract bool Remove() | |
| C++/CLI | |
|---|---|
public: abstract bool Remove(); | |
Return Value
True, if the SSBlock was removed from the collection.Note the first element in the collection cannot be removed because it is the primary SSBlock.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA Ver 28.00