Keysight 89600 VSA .NET API
Remove(SSBlock) Method
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace > SSBlockCollection Class > Remove Method : Remove(SSBlock) Method


item
SSBlock to remove from the collection

Glossary Item Box

Removes the indicated SSBlock from the collection.

Syntax

Visual Basic (Declaration) 
Public Overloads MustOverride Function Remove( _
   ByVal item As SSBlock _
) As Boolean
C# 
public abstract bool Remove( 
   SSBlock item
)
C++/CLI 
public:
abstract bool Remove( 
   SSBlock^ item
) 

Parameters

item
SSBlock to remove from the collection

Return Value

True, if the SSBlock was removed from the collection.

Remarks

Note the first element in the collection cannot be removed because it is the primary SSBlock.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also