Keysight 89600 VSA .NET API
SSBlockSymbolStart Enumeration
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace : SSBlockSymbolStart Enumeration


Glossary Item Box

Enum value indicates the symbol start equation used when the numerology is 30 kHz (µ = 1).

Syntax

Visual Basic (Declaration) 
Public Enum SSBlockSymbolStart 
   Inherits System.Enum
C# 
public enum SSBlockSymbolStart : System.Enum 
C++/CLI 
public enum class SSBlockSymbolStart : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
Option1Symbol start option 1 ({4,8,16,20}+28*n).—
Option2Symbol start option 2 ({2,8}+14*n).—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 23.00

See Also