Keysight 89600 VSA .NET API
Create Method
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace > SrsCollection Class : Create Method


Glossary Item Box

Creates a new SRS channel and appends it to the collection.

Syntax

Visual Basic (Declaration) 
Public MustOverride Function Create() As Srs
C# 
public abstract Srs Create()
C++/CLI 
public:
abstract Srs^ Create(); 

Return Value

A handle to the new SRS.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also