Keysight 89600 VSA .NET API
SrsRepetitionFactor Enumeration
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace : SrsRepetitionFactor Enumeration


Glossary Item Box

Enum values indicating the repetition factor of SRS channels

Syntax

Visual Basic (Declaration) 
Public Enum SrsRepetitionFactor 
   Inherits System.Enum
C# 
public enum SrsRepetitionFactor : System.Enum 
C++/CLI 
public enum class SrsRepetitionFactor : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
N1Specifies SRS repetition factor as 1 (N1).—
N12Specifies SRS repetition factor as 12 (N12).26.00
N2Specifies SRS repetition factor as 2 (N2).—
N4Specifies SRS repetition factor as 4 (N4).—
N8Specifies SRS repetition factor as 8 (N8).26.00
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 25.00

See Also