Keysight 89600 VSA .NET API
SrsResourceType Enumeration
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace : SrsResourceType Enumeration


Glossary Item Box

Enum values indicating the resource type of SRS channels

Syntax

Visual Basic (Declaration) 
Public Enum SrsResourceType 
   Inherits System.Enum
C# 
public enum SrsResourceType : System.Enum 
C++/CLI 
public enum class SrsResourceType : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
AperiodicSpecifies resource type as aperiodic.—
CustomDefinedSpecifies resource type as customer defined, which is a slot array and VSA assumes this allocation repeats in every frame.—
PeriodicSpecifies resource type as periodic.—
SemiPersistentSpecifies resource type as semi-persistent.—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 25.00

See Also