| Visual Basic (Declaration) | |
|---|---|
Public MustOverride Property CombOffset As Integer | |
| C# | |
|---|---|
public abstract int CombOffset {get; set;} | |
Property Value
The value ranges from 0 to combValue - 1, where combValue = 2 if equals to , and combValue = 4 if equals to . The default value is 0.According to TS38.211 6.4.1.4.3, this value decides the comb offset on which this SRS is transmitted/>, .
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA Ver 25.00