Keysight 89600 VSA .NET API
FlexibleSymbols Property
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace > Srs Class : FlexibleSymbols Property


Glossary Item Box

Gets or sets the flexible symbols to be used in the slot format.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property FlexibleSymbols As Integer
C# 
public abstract int FlexibleSymbols {get; set;}
C++/CLI 
public:
abstract property int FlexibleSymbols {
   int get();
   void set (    int value);
}

Property Value

The default is 0, indicating no "Flexible" symbols should be allocated to this physical channel.

Remarks

This property helps define the set of symbols reserved for this CSI-RS physical channel. This value represents a bitmap to indicate which "Flexible" symbols from the Sfi should be available to this CSI-RS physical channel (in every slot). This is applied in coordination with Sfi.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 25.00

See Also