| Visual Basic (Declaration) | |
|---|---|
Public MustOverride Property FrequencyDomainPosition As Integer | |
| C# | |
|---|---|
public abstract int FrequencyDomainPosition {get; set;} | |
Property Value
The value ranges from 0 to 67. The default value is 0.According to TS38.211 6.4.1.4.3, this value along with other parameters decides the frequency position index when frequency hopping is enabled or disabled.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA Ver 25.00