Keysight 89600 VSA .NET API
FrequencyDomainShift Property
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace > Srs Class : FrequencyDomainShift Property


Glossary Item Box

Gets or sets a value indicating the frequency domain shift of this physical channel.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property FrequencyDomainShift As Integer
C# 
public abstract int FrequencyDomainShift {get; set;}
C++/CLI 
public:
abstract property int FrequencyDomainShift {
   int get();
   void set (    int value);
}

Property Value

The value ranges from 0 to 268. The default value is 0.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 25.00

See Also