Gets or sets a value indicating the frequency scaling factor.
Syntax
| Visual Basic (Declaration) | |
|---|
Public Overridable Property FrequencyScalingFactor As Integer |
| C# | |
|---|
public virtual int FrequencyScalingFactor {get; set;} |
| C++/CLI | |
|---|
public:
virtual property int FrequencyScalingFactor {
int get();
void set ( int value);
} |
Property Value
The default value is 1.
Requirements
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA
Ver 28.40
See Also