Keysight 89600 VSA .NET API
SubcarrierSpacingCommon Enumeration
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace : SubcarrierSpacingCommon Enumeration


Glossary Item Box

Enum values indicating the subcarrierSpacingCommon as defined in the 3GPP-NR specification.

Syntax

Visual Basic (Declaration) 
Public Enum SubcarrierSpacingCommon 
   Inherits System.Enum
C# 
public enum SubcarrierSpacingCommon : System.Enum 
C++/CLI 
public enum class SubcarrierSpacingCommon : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
Scs15Or60Numerology of 15 kHz subcarrier scaling for FR1 and 60kHz for FR2.—
Scs30Or120Numerology of 30 kHz subcarrier scaling for FR1 and 120kHz for FR2.—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Remarks

This value is defined in PBCH MIB (master information block). It indicates the subcarrier spacing used for the initial BWP, SIB1, Msg.2/4 for initial access, paging and broadcast SI-messages. If the UE acquires this MIB on a carrier frequency lower than 6GHz, the value scs15or60 corresponds to 15 KHz and the value scs30or120 corresponds to 30 KHz. If the UE acquires this MIB on a carrier frequency higher than 6GHz, the value scs15or60 corresponds to 60 KHz and the value scs30or120 corresponds to 120 KHz.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 24.20

See Also