Keysight 89600 VSA .NET API
SymbolPhaseCompensationSource Enumeration
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace : SymbolPhaseCompensationSource Enumeration


Glossary Item Box

Enum values indicating frequency value to use for per-symbol phase compensation.

Syntax

Visual Basic (Declaration) 
Public Enum SymbolPhaseCompensationSource 
   Inherits System.Enum
C# 
public enum SymbolPhaseCompensationSource : System.Enum 
C++/CLI 
public enum class SymbolPhaseCompensationSource : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
DisabledPer-symbol phase compensation is disabled.—
ManualUse ComponentCarrier.SymbolPhaseCompensationManualFrequency.—
MeasurementUse carrier center frequency.—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 23.20

See Also