Keysight 89600 VSA .NET API
SynchronizationSource Enumeration
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace : SynchronizationSource Enumeration


Glossary Item Box

Enum values indicating the channel source used for initial synchronization

Syntax

Visual Basic (Declaration) 
Public Enum SynchronizationSource 
   Inherits System.Enum
C# 
public enum SynchronizationSource : System.Enum 
C++/CLI 
public enum class SynchronizationSource : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
AllSignalsSpecifies the channel source used for initial synchronization includes all the signals configured.30.00
AutoSpecifies the channel source used for initial synchronization is auto selected.—
CsirsSpecifies the channel source used for initial synchronization is CSI-RS.28.00
NotProvidedThe data is already synchronized by the data provider before sending to VSA, so no channel is used for initial synchronization.29.00
PdcchDmrsSpecifies the channel source used for initial synchronization is PDCCH DMRS.—
PdschDmrsSpecifies the channel source used for initial synchronization is PDSCH DMRS.—
PrachSpecifies the channel source used for initial synchronization is PRACH.—
PrsSpecifies the channel source used for initial synchronization is Positioning Reference Signal (PRS).29.40
PucchDmrsSpecifies the channel source used for initial synchronization is PUCCH DMRS.—
PuschDmrsSpecifies the channel source used for initial synchronization is PUSCH DMRS.—
SrsSpecifies the channel source used for initial synchronization is SRS.—
SsbSpecifies the channel source used for initial synchronization is SSB.—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 27.00

See Also